Working with third party libraries

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Working with third party libraries

809 次查看
chandraevolute
Contributor V

Yuri
Hi ,

I am using third part source files, cross compiling them and generating the shared library.

I am using imx6ulevk, poky version 1.8. I am able to generate the shared libraries.

And i wrote a sample application using the shared library and crosscompiled and generated the executable.

When I am trying to run the executable say

./Example it is giving a error like libMso.so cannot be opened . File is missing.

I copied the libraries to /usr/lib/ still the error comes.

Do i need to build the RFS again by copying these libraries ??

0 项奖励
回复
1 回复

747 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please try the following :

$ file ./Example

and

$ ldd ./Example

and let me look at the log.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复