How to control the SNVS_LPCR Register(TOP, DP_EN bit).

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to control the SNVS_LPCR Register(TOP, DP_EN bit).

2,769 Views
changyonglee
Contributor II

Dear All.

We connect i.MX6SL PMIC_ON_REQ pin to PMIC(PF0100) PWRON pin.

and we board battery.

sudden poweroff -> how to register setting.?  ex) disconnect power adapter.

0 Kudos
Reply
4 Replies

2,425 Views
dhvanil_patel1
Senior Contributor I

HI,

We want to auto power on the i.MX6ul board without any user interaction. Is  it possible to implement this mechanism on imx6 evk

-

Dhvanil

0 Kudos
Reply

2,425 Views
art
NXP Employee
NXP Employee

Not on the current version of the i.MX6UL EVK board.

Artur

0 Kudos
Reply

2,425 Views
changyonglee
Contributor II

hi Artur Petukhov.

case 1) boot -> onoff button use power off (SNVS_LP Control Register is TOP bit 1 set) -> no automatic power on.

case 2) boot -> "poweroff" linux command use power off (SNVS_LP Control Register is TOP bit 1 set) -> no automatic power on.

case 2) boot -> power adapter remove.  power off (SNVS_LP Control Register is TOP bit 1 not set) -> automatic power on.

how I can fix this? I do not need automatic power on. only on off button.

refencence manual please.

I hope it helps. Regards,

Thanks!

0 Kudos
Reply

2,425 Views
art
NXP Employee
NXP Employee

Do you have a pullup on the PMIC PWRON pin? If not, pull it up to the VDD_SNVS_IN voltage by a 10kOhm resistor.


Have a great day,
Artur

0 Kudos
Reply