Wireless printing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wireless printing

1,898件の閲覧回数
EmbeddedTech
Contributor III

Hi,

I am using iMXRT1060 EVK and ublox wifi+BLE module. I would like to connect to the wireless printer and print from my iMXRT host +ublox module. Is there any example code for this in the SDK?

Thanks.

0 件の賞賛
返信
3 返答(返信)

1,886件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @EmbeddedTech ,

  As I know, we don't have the detail application about the BLE printer, but you can check your BLE printer, which detail BLE method it is using.

All the RT1060 bluetooth code is in the SDK:

\SDK_2_10_1_EVK-MIMXRT1060\boards\evkmimxrt1060\edgefast_bluetooth_examples

You can check it.

 

Wish it helps you!

Best Regards,

Kerry

0 件の賞賛
返信

1,877件の閲覧回数
EmbeddedTech
Contributor III

Hi Kerry,

I want to connect to a wireless printer and not BLE printer. Is there any reference for that?

Thanks. 

0 件の賞賛
返信

1,864件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @EmbeddedTech ,

   Thanks for your information.

  So, if your pinter already supports the wifi, you can use the wifi method.

   Today, I help you to check with wifi expert, and also get some information which may useful to you.

   Your ublox is using the NXP 88W8987 chip, right? Then, you can use the SDK wifi client to connect your printer. Please check this SDK code:

SDK_2_10_1_MIMXRT1060-EVKB\boards\evkbmimxrt1060\wifi_examples\wifi_cli

 After the connection, you need to find some network driver for your pinter, then migrate it to the RT SDK to driver your printer.

But, please note, we don't have the examples or application, the above is the thought, our expert told me the linux driver contains the network printer driver, you can migrate it by yourself. You also need to find your used printer matched driver.

 

Wish it helps you!

Best Regards,

Kerry

 

0 件の賞賛
返信