Windows Embedded Compact 7 i.MX6 Find Applications Core

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Windows Embedded Compact 7 i.MX6 Find Applications Core

1,554 Views
kriszawada
Contributor III

I am using the Freescale SABRE MCIMX6Q-SD and Windows Embedded Compact 7 that is running two Qt applications.

Is there a way to determine within the software how many cores the OS is utilizing?

Is there a way to determine which core my applications are being executed on?

Is there a way to start my application and assign it to specific core?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,472 Views
Yuri
NXP Employee
NXP Employee

  I hope the following helps.

http://social.technet.microsoft.com/wiki/contents/articles/14942.smp-verification-on-wec-7-with-i-mx...


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply