Windows Embedded Compact 7 i.MX6 Find Applications Core

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Windows Embedded Compact 7 i.MX6 Find Applications Core

1,027 次查看
kriszawada
Contributor III

I am using the Freescale SABRE MCIMX6Q-SD and Windows Embedded Compact 7 that is running two Qt applications.

Is there a way to determine within the software how many cores the OS is utilizing?

Is there a way to determine which core my applications are being executed on?

Is there a way to start my application and assign it to specific core?

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

945 次查看
Yuri
NXP Employee
NXP Employee

  I hope the following helps.

http://social.technet.microsoft.com/wiki/contents/articles/14942.smp-verification-on-wec-7-with-i-mx...


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复