Windows 10 IoT Enterprise for UART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Windows 10 IoT Enterprise for UART

Jump to solution
2,706 Views
hankwang
Contributor V

Hi, I have an 8MP processor and the UART1 and UART 2 pin designs are the same as the EVK board.

The only difference is that my motherboard doesn't have CTS/RTS.

I tested UART1 loopback and couldn't get the data.

I use UART2 to communicate with the laptop, UART2 can communicate with the laptop.

The difference between UART1 and UART2 is RTS/CTS.

About RTS/CTS of UART1. Where can I disable it for UART1?

 

 

0 Kudos
Reply
1 Solution
2,660 Views
hankwang
Contributor V

Hi @michal_hromadka  Sorry, no problem with UART. The problem is that my motherboard is broken.I changed the board and UART communication is good.

View solution in original post

0 Kudos
Reply
3 Replies
2,661 Views
hankwang
Contributor V

Hi @michal_hromadka  Sorry, no problem with UART. The problem is that my motherboard is broken.I changed the board and UART communication is good.

0 Kudos
Reply
2,654 Views
michal_hromadka
NXP Employee
NXP Employee

Hello @hankwang ,

thank you for the update. 

Have a nice day.

 

Best regards,

Michal

0 Kudos
Reply
2,689 Views
michal_hromadka
NXP Employee
NXP Employee

Hello @hankwang,

 

Could you please describe how you tested the loopback with UART1? 
By default the UART1 is not enabled in Win IoT BSP. Did you enable it in the BSP source codes?

 

Best regards,

Michal

0 Kudos
Reply