Windows 10 IoT Enterprise for UART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Windows 10 IoT Enterprise for UART

ソリューションへジャンプ
1,716件の閲覧回数
hankwang
Contributor V

Hi, I have an 8MP processor and the UART1 and UART 2 pin designs are the same as the EVK board.

The only difference is that my motherboard doesn't have CTS/RTS.

I tested UART1 loopback and couldn't get the data.

I use UART2 to communicate with the laptop, UART2 can communicate with the laptop.

The difference between UART1 and UART2 is RTS/CTS.

About RTS/CTS of UART1. Where can I disable it for UART1?

 

 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,670件の閲覧回数
hankwang
Contributor V

Hi @michal_hromadka  Sorry, no problem with UART. The problem is that my motherboard is broken.I changed the board and UART communication is good.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,671件の閲覧回数
hankwang
Contributor V

Hi @michal_hromadka  Sorry, no problem with UART. The problem is that my motherboard is broken.I changed the board and UART communication is good.

0 件の賞賛
返信
1,664件の閲覧回数
michal_hromadka
NXP Employee
NXP Employee

Hello @hankwang ,

thank you for the update. 

Have a nice day.

 

Best regards,

Michal

0 件の賞賛
返信
1,699件の閲覧回数
michal_hromadka
NXP Employee
NXP Employee

Hello @hankwang,

 

Could you please describe how you tested the loopback with UART1? 
By default the UART1 is not enabled in Win IoT BSP. Did you enable it in the BSP source codes?

 

Best regards,

Michal

0 件の賞賛
返信