Windows 10 Enterprise 3-Display Error using W1.5.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Windows 10 Enterprise 3-Display Error using W1.5.0

ソリューションへジャンプ
16,662件の閲覧回数
hankwang
Contributor V

Hey, I'm trying to display screen on HDMI, LVDS and MIPI DSI on an 8MP EVK board. But the 8MP EVK board only display screen on LVDS and HDMI at start up to windows.

But I'm sure MIPI DSI is good. Because when Windows boots into Windows, the first display is MIPI DSI and then changes to LVDS and HDMI.

 

There are two problem:

1. I receive an error message when trying to enter Windows. (Attached file (Error Message.jpg) is the error message.). This message is displayed on both HDMI and LVDS.

2. MIPI DSI shows nothing when preparing to enter Windows. (Attached file(MIPI_DSI_HDMI.png) is same as my cable)

The attachment (galcore.txt) is my INF file. Please help to check if there is any error?

ラベル(1)
0 件の賞賛
返信
1 解決策
16,615件の閲覧回数
Michal_Minarcik
NXP Employee
NXP Employee

Hello @hankwang,

To enable 3 displays on 8MP EVK board, please follow the procedure below:

1. Use default Galcore.inf file (without the edits you sent)

2. Install the OS preferably with one display connected (default HDMI)

3. Connect the second and third displays to the board

4. Copy the contents of the .zip file that is attached to the board

5. Run LVDS0_HDMI_MIPI0_multimon.reg to enable multi-monitor mode, restart the board

6. All 3 displays should be active as follows (also the picture in the attachment) 

Display 1 a Display 3 are duplicated, Display 2 is extended

1 - LVDS0
2 - MIPI DSI
3 - HDMI

7. To reverts the registry settings, run HDMI_multimon.reg, then restart the board

8. Only 1 (HDMI display) display will work

 

Best regards,

Michal

 

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
16,616件の閲覧回数
Michal_Minarcik
NXP Employee
NXP Employee

Hello @hankwang,

To enable 3 displays on 8MP EVK board, please follow the procedure below:

1. Use default Galcore.inf file (without the edits you sent)

2. Install the OS preferably with one display connected (default HDMI)

3. Connect the second and third displays to the board

4. Copy the contents of the .zip file that is attached to the board

5. Run LVDS0_HDMI_MIPI0_multimon.reg to enable multi-monitor mode, restart the board

6. All 3 displays should be active as follows (also the picture in the attachment) 

Display 1 a Display 3 are duplicated, Display 2 is extended

1 - LVDS0
2 - MIPI DSI
3 - HDMI

7. To reverts the registry settings, run HDMI_multimon.reg, then restart the board

8. Only 1 (HDMI display) display will work

 

Best regards,

Michal

 

0 件の賞賛
返信
16,583件の閲覧回数
hankwang
Contributor V

Hi , thanks for the information. The 8MP EVK board can display 3 screens.

But I have a problem, although 3 screens can be displayed independently, there will be lag or confusion in 2 or 1 screen (Just like the picture below). When I set up 2 screens to sync and expand one screen. All screens are good. 

 So is it not allowed to display three screens independently?

 

lags.jpg

0 件の賞賛
返信
16,419件の閲覧回数
Michal_Minarcik
NXP Employee
NXP Employee

Hi @hankwang,

To set 3 displays independently, please follow below instructions:

Open regedit (Registry Editor) as Administrator and navigate to: 

HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Control\Class\{4d36e968-e325-11ce-bfc1-08002be10318}\0000

and change GdiAccLevel to 0

Then reboot the board and 3 displays can be displayed independently (extended).

Best regards,

Michal

0 件の賞賛
返信
16,402件の閲覧回数
hankwang
Contributor V

Thanks for your reply. We'll give it a try.

0 件の賞賛
返信
16,477件の閲覧回数
Michal_Minarcik
NXP Employee
NXP Employee

Hi @hankwang,

We test how the displays work with each other. Please give us a few days to test.

Best regards,

Michal

0 件の賞賛
返信
16,642件の閲覧回数
michal_hromadka
NXP Employee
NXP Employee

@Michal_Minarcik Can you help here, please ?

0 件の賞賛
返信