WiFi module integration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WiFi module integration

1,813 Views
gbassi1
Contributor II

I cannot make the Toradex Colibri iMX6ULL Wifi Module work using fsl repo.

After the image is running, there is not even any wireless interface detected when I try "ip a" or "ifconfig"

To begin with, how can I make the Wireless interface visible to the OS?

From Toradex repo I could learn that the wifi used is mwifiex

The Carrier board i'm using is: Aster V1.1B

The uP board is: Colibri imx6ull 512MB w/ WIFI (product id 0040....)

Thanks

Labels (1)
0 Kudos
Reply
1 Reply

1,731 Views
igorpadykov
NXP Employee
NXP Employee

Hi Gaston

one can look at toradex wifi solutions:

Wi-Fi 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply