WiFi module integration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

WiFi module integration

1,833件の閲覧回数
gbassi1
Contributor II

I cannot make the Toradex Colibri iMX6ULL Wifi Module work using fsl repo.

After the image is running, there is not even any wireless interface detected when I try "ip a" or "ifconfig"

To begin with, how can I make the Wireless interface visible to the OS?

From Toradex repo I could learn that the wifi used is mwifiex

The Carrier board i'm using is: Aster V1.1B

The uP board is: Colibri imx6ull 512MB w/ WIFI (product id 0040....)

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

1,751件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Gaston

one can look at toradex wifi solutions:

Wi-Fi 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信