WiFi chipset supporting AP mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

WiFi chipset supporting AP mode

2,373件の閲覧回数
jaffinmk
Contributor III

Hello all

I am in search of a Wifi chipset which can be interfaced with iMX6 QuadPlus Sabre board easily (I am running linux 3.14) and which supports dual band frequency and AP mode and has a good performance. I have found BCM4330 chipset. Is there any other better option. Also is there any USB adapter with BCM4330 to connect with the board and test it out before buying the chipset. Any information regarding this will be helpful.

ラベル(2)
0 件の賞賛
返信
1 返信

2,139件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jaffin

L3.14.xx early versions supported Atheros AR6003 please refer to attached

Linux Manual Chapter 48 AR6003 WiFi.

http://www.nxp.com/webapp/Download?colCode=L3.14.28_1.0.0_LINUX_DOCS&Parent_nodeId=13376994810717061... 

for broadcom wifi options one can check

https://wikidevi.com/wiki/Broadcom#USB 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信