SD Bus Driver Issue on IMX51 WEC7 BSP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SD Bus Driver Issue on IMX51 WEC7 BSP

2,226 次查看
prabhur
Contributor I

Hi All,

I have build the IMX51 WEC7  BSP in release mode using the solution file provided along with the BSP. As mentioned in the user guide section 5.3.3(Program EBOOT in SD/MMC Card Using ATK Tool) i have flashed the eboot.nb0 into the SD/MMC card through USB in bootstrap mode. After flashing the eboot i changed the switch setting to Boot mode and configured the boot menu as follows,

-----------------------------------------------------------------------------
Freescale iMX SOC Menu Item
-----------------------------------------------------------------------------
[0] IP Address : 192.168.5.24
[1] Set IP Mask : 255.255.255.0
[2] Boot Delay : 3
[3] DHCP : Disabled
[4] Reset to Factory Default Configuration
[5] Select Boot Device : NK from SD/MMC
[6] Set MAC Address : ff-ff-ff-ff-ff-ff
[7] Format OS NAND Region
[8] Format All NAND Regions
[9] Bootloader Shell
[I] KITL Work Mode : Interrupt
[K] KITL Enable Mode : Enable
[P] KITL Passive Mode : Disable
[S] Save Settings
[D] Download Image Now
[L] Launch Existing Flash Resident Image Now
[E] Select Ether Device : FEC
[M] MMC and SD Utilities : ESDHC[1] is activated

After saving the configuration i have chosen the option Download Image Now) and the eboot starts sending bootme packet to the host.In the VS2008 solution file i did Target -> attach device and the image gets downloaded through ethernet. After reset i have chosen option L(Launch Existing Flash Resident Image Now) and the image gets booted.After some time i faced the following error and the boot got hanged.It seems like some issue with SD Bus driver.

Can someone help me to resolve this issue?

9359 PID:400002 TID:2db0006 SDSynchronousBusRequest_I: queue request failed(0xc0000014),TransferClass(2), CommandCode(5),CommandArgument(0)
9359 PID:400002 TID:2db0006 SDBUS:Cur Req failed, complete rest of them
9359 PID:400002 TID:2db0006 SDSynchronousBusRequest_I: queue request failed(0xc0000014),TransferClass(2), CommandCode(1),CommandArgument(400e0000)
9359 PID:400002 TID:2db0006 SDBUS:Cur Req failed, complete rest of them

11680 PID:400002 TID:ba0006 OTG : Load HCD
11916 PID:400002 TID:ba0006 OTG : Unload HCD
14047 PID:400002 TID:ba0006 OTG : Load UFN
20198 PID:41e003e TID:515006a Event is successfully created 1ab0807

Full log upto hang issue:

PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NK.EXE'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\KERNEL.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\KITL.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\HD.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\OSAXST0.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\OSAXST1.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.COREDLL.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\KD.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\FILESYS.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\FSDMGR.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ROMFSD.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.LOCALE.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.NORMALIZE.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RELFSD.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DEVICE.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DEVMGR.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.CEDDK.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\PM.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\BUSENUM.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CSPDDK.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CCFGSVC.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\BCRYPT.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.SQLCESE35.SYS.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.FPCRT.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.OLE32.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.SORTING.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\COREDLL.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\OALIOCTL.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SHELL.EXE'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\LOCALE.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NORMALIZE.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\TOOLHELP.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NLEDDRVR.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ALPCD.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\TAPI.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DLLHEAPINFOEXT.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RELFSDEXT.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\UDEVICE.EXE'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SOFTKB.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\UDEVICE.EXE'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\OLE32.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RPCRT4LEGACY.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\LPCRT.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\BCRYPT.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NOTIFY.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NTLMSSP_SVC.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RSAENH.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ECSPI.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\IPUV3_BASE.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\I2C.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\PMICPDK_MC13892.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ECSPISDK.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\BATTERY.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\VPU.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WAVEDEV2_SGTL5000.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.MMTIMER.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\I2CSDK.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\PMICSDK_MC13892.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WAVEAPI.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CREDSVC.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CREDPROV.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NTLMSSP.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SCARD.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.WINSCARD.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SDBUS.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\HCD_HSH1.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.USBD.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\PP.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\VDI.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CAMERA.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NDIS.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.CXPORT.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NETIO.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.RPCRT4.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\VMINI.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RSAENH.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ASYNCMAC.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\VEIM.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.DHCPSRV.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NWIFI.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ESDHC.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\AFD.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\PPP.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WS2K.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\TCPIP.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\AUTORAS.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.IPHLPAPI.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\TCPIPREG.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WS2INSTL.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DHCP.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.WS2.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DHCPV6.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.SSLLSP.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.WSPM.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.EAP.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NDISUIO.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NDISPWR.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ETHMAN.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\IPHLPAPI.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WINNSI.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RPCRT4.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NSI.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WS2.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CXPORT.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WS2SERV.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\FSL_USBOTG.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\USB_GIISR.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SDMEMORY.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\MSPART.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\EXFAT.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DISKCACHE.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CACHEFILT.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\USBMSC.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\USBDISK6.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\USBFN.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SERIALUSBFN.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\TOUCH.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\BTD.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\BTHUNIV.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\UNIMODEM.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\PPU.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NSIPROXY.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\EAP3SVC.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NSISVC.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\EAPSVC.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CMSERVICE.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RMNET.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RSPBASIC.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CMCSPRAS.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WLANSVC.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\OLEAUT32.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\FPCRT.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ONEX.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\EAPPPRXY.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\EAPPCFG.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WLANMSM.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WLANSEC.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WLANUTIL.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CMCSPIP.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\REDIR.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SSLLSP.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WSPM.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NETBIOS.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\PWRBUTTON.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\AMDGSLLDD.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\LIBGSL.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\LIBKOS.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\LIBGSLMEMCFG.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\GWES.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.WAVEAPIC.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DDRAW_IPU.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\LIB2DZ160K.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\LIBGSLWRAPPERK.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\MGTT_O.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\KBDMOUSE.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\GWEUSER.EXE'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\TCHPROXY.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\TCHCALDLL.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SORTING.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\MSIM.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\EXPLORER.EXE'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WAVEAPIC.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DMSRV.EXE'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\COMMCTRL.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CESHELL.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SHLWAPI.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SHCORE.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DMSAPI.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SERVICESENUM.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\OSSVCS.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\OMADMSVC.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SERVICESD.EXE'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\METABASESERVICE.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SERVICESFILTER.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\LPCD.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DCOMSSD.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WINSOCK.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SECUR32.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SCHANNEL.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CRYPT32.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\MSASN1.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NCRYPT.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\UPNPSVC.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\UPNPCAPI.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WININET.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SPNEGO.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\AYGSHELL.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\LASSD.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CEDDK.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\LAP_PW.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\IMAGING.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\HTTPD.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ZLIB.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\BTSVC.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\BTDRT.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NETUI.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\OBEXSRVR.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\UPNPLOADER.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\UPNPHOST.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ATHSRVC.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DSTSVC.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\PROXYSVC.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CMNET.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\REGEXTDEV.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\MLWD.EXE'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ML.EXE'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\MLIBDLL.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\XMLLITE.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SQLCEOLEDB35.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SQLCEER35EN.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SQLCESE35.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SQLCEQP35.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\UPNPCTRL.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NK.EXE'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\KERNEL.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\KITL.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\HD.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\OSAXST0.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\OSAXST1.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.COREDLL.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\KD.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\FILESYS.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\FSDMGR.DLL'
3528 PID:400002 TID:5d0002 OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ROMFSD.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.LOCALE.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.NORMALIZE.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RELFSD.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DEVICE.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DEVMGR.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.CEDDK.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\PM.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\BUSENUM.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CSPDDK.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CCFGSVC.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\BCRYPT.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.SQLCESE35.SYS.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.FPCRT.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.OLE32.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.SORTING.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\COREDLL.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\OALIOCTL.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SHELL.EXE'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\LOCALE.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NORMALIZE.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\TOOLHELP.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NLEDDRVR.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DLLHEAPINFOEXT.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RELFSDEXT.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ALPCD.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\TAPI.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\UDEVICE.EXE'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SOFTKB.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\UDEVICE.EXE'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\OLE32.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RPCRT4LEGACY.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\LPCRT.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\BCRYPT.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NTLMSSP_SVC.DLL'
PB Debugger Loaded 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RSAENH.DLL', no matching symbolic information found.
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NOTIFY.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ECSPI.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\IPUV3_BASE.DLL'
5914 PID:400002 TID:ba0006 IpuBufferManagerInit(): Detected reserved video memory(67108864 bytes), will ignore registry setting!
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\I2C.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\PMICPDK_MC13892.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ECSPISDK.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\BATTERY.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\VPU.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WAVEDEV2_SGTL5000.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.MMTIMER.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\I2CSDK.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\PMICSDK_MC13892.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WAVEAPI.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CREDSVC.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CREDPROV.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NTLMSSP.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SCARD.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.WINSCARD.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.SIM.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.SIM.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SDBUS.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\HCD_HSH1.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.USBD.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\PP.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\VDI.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CAMERA.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NDIS.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.CXPORT.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NETIO.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.RPCRT4.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RNDISFN.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RNDISFN.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RNDISFN.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RNDISFN.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\VMINI.DLL'
PB Debugger Loaded 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RSAENH.DLL', no matching symbolic information found.
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ASYNCMAC.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\VEIM.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.DHCPSRV.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NWIFI.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\FEC.DLL'
8454 PID:400002 TID:ba0006 FEC already in use for KITL. Driver load failure!
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\FEC.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ESDHC.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\AFD.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\PPP.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WS2K.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\TCPIP.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\AUTORAS.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.IPHLPAPI.DLL'
8887 PID:400002 TID:2190002 UsbHost : New Hub [address(1) / layer(0)]
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\TCPIPREG.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WS2INSTL.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\BTD.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\BTHUNIV.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\BTD.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\BTHUNIV.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.SSLLSP.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.WS2.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.WS2.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.SSLLSP.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DHCP.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.WS2.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DHCPV6.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.SSLLSP.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.WSPM.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.EAP.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NDISUIO.DLL'
9359 PID:400002 TID:2db0006 SDSynchronousBusRequest_I: queue request failed(0xc0000014),TransferClass(2), CommandCode(5),CommandArgument(0)
9359 PID:400002 TID:2db0006 SDBUS:Cur Req failed, complete rest of them
9359 PID:400002 TID:2db0006 SDSynchronousBusRequest_I: queue request failed(0xc0000014),TransferClass(2), CommandCode(1),CommandArgument(400e0000)
9359 PID:400002 TID:2db0006 SDBUS:Cur Req failed, complete rest of them
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NDISPWR.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ETHMAN.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\IPHLPAPI.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WINNSI.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RPCRT4.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NSI.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WS2.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CXPORT.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WS2SERV.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\FSL_USBOTG.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\USB_GIISR.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SDMEMORY.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\MSPART.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\EXFAT.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DISKCACHE.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CACHEFILT.DLL'
11680 PID:400002 TID:ba0006 OTG : Load HCD
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\HCD_HSOTG.DLL'
11916 PID:400002 TID:ba0006 OTG : Unload HCD
11963 PID:400002 TID:24e000a UsbHost : New Function [address(2) / layer(1)]
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\USBMSC.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\USBDISK6.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\HCD_HSOTG.DLL'
14047 PID:400002 TID:ba0006 OTG : Load UFN
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\USBFN.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SERIALUSBFN.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\TOUCH.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\BTD.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\BTHUNIV.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\UNIMODEM.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\PPU.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NSIPROXY.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\EAP3SVC.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NSISVC.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\EAPSVC.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CMSERVICE.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RMNET.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RSPCELLULAR.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RSPCELLULAR.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\RSPBASIC.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CMCSPRAS.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WLANSVC.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\OLEAUT32.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\FPCRT.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ONEX.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\EAPPPRXY.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\EAPPCFG.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WLANMSM.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WLANSEC.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WLANUTIL.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CMCSPIP.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SSLLSP.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WSPM.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\REDIR.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NETBIOS.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\PWRBUTTON.DLL'
PB Debugger Loaded 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\AMDGSLLDD.DLL', no matching symbolic information found.
PB Debugger Loaded 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\LIBGSL.DLL', no matching symbolic information found.
PB Debugger Loaded 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\LIBKOS.DLL', no matching symbolic information found.
PB Debugger Loaded 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\LIBGSLMEMCFG.DLL', no matching symbolic information found.
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\GWES.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\K.WAVEAPIC.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DDRAW_IPU.DLL'
PB Debugger Loaded 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\LIB2DZ160K.DLL', no matching symbolic information found.
PB Debugger Loaded 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\LIBGSLWRAPPERK.DLL', no matching symbolic information found.
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\MGTT_O.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\KBDMOUSE.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\KBDUS.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\KBDUS.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\KBDUS.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\KBDUS.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\KBDUS.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\KBDUS.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\KBDUS.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\KBDUS.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\GWEUSER.EXE'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\TCHPROXY.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\TCHCALDLL.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SORTING.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\MSIM.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\EXPLORER.EXE'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WAVEAPIC.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\COMMCTRL.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DMSRV.EXE'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CESHELL.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SHLWAPI.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SHCORE.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SERVICESSTART.EXE'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DMSAPI.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\OSSVCS.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SERVICESENUM.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\OMADMSVC.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SERVICESD.EXE'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\METABASESERVICE.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SERVICESFILTER.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\LPCD.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DCOMSSD.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WINSOCK.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SECUR32.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SCHANNEL.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CRYPT32.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\MSASN1.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NCRYPT.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\UPNPSVC.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\UPNPCAPI.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\WININET.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SPNEGO.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\AYGSHELL.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\LASSD.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CEDDK.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\LAP_PW.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\IMAGING.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ZLIB.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\HTTPD.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\BTSVC.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\BTDRT.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\NETUI.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\OBEXSRVR.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\UPNPLOADER.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\UPNPHOST.DLL'
PB Debugger Loaded 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ATHSRVC.DLL', no matching symbolic information found.
20198 PID:41e003e TID:515006a Event is successfully created 1ab0807
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\DSTSVC.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\PROXYSVC.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\CMNET.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\REGEXTDEV.DLL'
PB Debugger Unloaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SERVICESSTART.EXE'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\MLWD.EXE'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\ML.EXE'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\MLIBDLL.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\XMLLITE.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SQLCEOLEDB35.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SQLCEER35EN.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SQLCESE35.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\SQLCEQP35.DLL'
PB Debugger Loaded symbols for 'C:\WINCE700\OSDESIGNS\IMX51_EVK_MOBILITY\RELDIR\FREESCALE_I_MX51_EVK_ARMV7_RELEASE\UPNPCTRL.DLL'

Regards,

Prabhu

标签 (1)
0 项奖励
回复
2 回复数

2,008 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please let me know more details about the issue :

 

1.
Is Your SD card meets the v2.1 spec ?

 

2.

 Is the HIVE used in the case ?

 

  The iMX53 will not boot correctly when the HIVE is enabled on a SD Card and the

FEC driver is included in the main OS.

The similar effect may take place for i.MX51.

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 项奖励
回复

2,008 次查看
prabhur
Contributor I

Hi Yuri,

1.The card which iam using was SDHC SanDisk 4(8GB).

2.I didnt enable hive on the SD card.
3.I tried removing FEC driver but no imapact.

Actually if iam trying to download and boot the image through ethernet(with KITL enabled) in release mode,the image got stuck after sometime.Not able to proceed forward.To get more debug logs i have build the driver in checked mode and tried to download the image,but download gets failure due to large size of the NK.bin.

Logs:

INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0xb
BSP Clock Configuration:
CKIH = 22579200 Hz
PLL1 = 800000000 Hz
PLL2 = 665000000 Hz
PLL3 = 216000000 Hz
LP_APM = 24000000 Hz
ARM = 800000000 Hz
AXI_A = 166250000 Hz
AXI_B = 133000000 Hz
EMI_SLOW = 133000000 Hz
AHB = 133000000 Hz
IPG = 66500000 Hz
PERCLK = 8000000 Hz
CKIL_SYNC = 32768 Hz
DDR = 200000000 Hz
ARM_AXI = 166250000 Hz
IPU_HSP = 133000000 Hz
VPU_AXI = 166250000 Hz
GPU = 166250000 Hz
GPU2D = 166250000 Hz
DEBUG_APB = 166250000 Hz
ENFC = 33250000 Hz
USBOH3 = 66500000 Hz
ESDHC1 = 47500000 Hz
ESDHC2 = 47500000 Hz
ESDHC3 = 47500000 Hz
ESDHC4 = 47500000 Hz
UART = 24000000 Hz
SSI1 = 5644800 Hz
SSI2 = 5644800 Hz
SSI3 = 5644800 Hz
SSI_EXT1 = 10285714 Hz
SSI_EXT2 = 10285714 Hz
USB_PHY = 24000000 Hz
TVE_216_54 = 216000000 Hz
DI = 27000000 Hz
VPU_RCLK = 24000000 Hz
SPDIF0 = 1142857 Hz
SPDIF1 = 1142857 Hz
SLIMBUS = 66500000 Hz
SIM = 66500000 Hz
FIRI = 24000000 Hz
HSI2C = 66500000 Hz
SSI_LP_APM = 22579200 Hz
SPDIF_XTAL = 24000000 Hz
HSC1 = 216000000 Hz
HSC2 = 216000000 Hz
ESC = 15428571 Hz
CSI_MCLK1 = 24629629 Hz
CSI_MCLK2 = 24629629 Hz
ECSPI = 66500000 Hz
LPSR = 0 Hz
PGC = 66500000 Hz
OSC = 24000000 Hz
CKIH_CAMP1 = 22579200 Hz
CKIH2_CAMP2 = 0 Hz
CKIH2 = 0 Hz
FPM = 33554432 Hz

Microsoft Windows CE Bootloader Common Library Version 1.4 Built Jan 2 2017 19:04:42
INFO: BoardID = 0x0.
CONTROLREG = 0x1f03011
CONFIGREG = 0x1000
OALPmicInit: silicon rev = 0x20
REV = 0x45d0
REG_SET0 = 0x20fd0
REG_MOD1 = 0x9
Microsoft Windows CE Ethernet Bootloader 1.0 for MX51 EVK (Jan 5 2017 10:12:50)
INFO: SBMR = 0xe0600003.
INFO: Bootloader launched from SD.
SD High Density card
SD: Switched to 4 bit mode
INFO: Initialized SD Card
SPIFMD_Init: Manufacturer ID = 0x1f270100
Page Size is 512 Bytes!
INFO: Initialized SPI Flash!
INFO: Loading boot configuration from SDHC
INFO: Successfully loaded boot configuration from SDHC
System ready!
Preparing for download...

Press [ENTER] to launch image stored in SD/MMC or [SPACE] to cancel.

Initiating image launch in 2 seconds.
-----------------------------------------------------------------------------
Freescale iMX SOC Menu Item
-----------------------------------------------------------------------------
[0] IP Address : 0.0.0.0
[1] Set IP Mask : 0.0.0.0
[2] Boot Delay : 3
[3] DHCP : Disabled
[4] Reset to Factory Default Configuration
[5] Select Boot Device : NK from SD/MMC
[6] Set MAC Address : ff-ff-ff-ff-ff-ff
[7] Format OS NAND Region
[8] Format All NAND Regions
[9] Bootloader Shell
[I] KITL Work Mode : Interrupt
[K] KITL Enable Mode : Disable
[P] KITL Passive Mode : Disable
[S] Save Settings
[D] Download Image Now
[L] Launch Existing Flash Resident Image Now
[E] Select Ether Device : USB Serial
[M] MMC and SD Utilities : ESDHC[1] is activated

After configuring I got following logs on the serial:

Selection: s
INFO: Storing boot configuration to SDHC
INFO: Successfully stored boot configuration to SDHC

-----------------------------------------------------------------------------
Freescale iMX SOC Menu Item
-----------------------------------------------------------------------------
[0] IP Address : 192.168.5.45
[1] Set IP Mask : 255.255.255.0
[2] Boot Delay : 3
[3] DHCP : Disabled
[4] Reset to Factory Default Configuration
[5] Select Boot Device : NK from SD/MMC
[6] Set MAC Address : ff-ff-ff-ff-ff-ff
[7] Format OS NAND Region
[8] Format All NAND Regions
[9] Bootloader Shell
[I] KITL Work Mode : Interrupt
[K] KITL Enable Mode : Enable
[P] KITL Passive Mode : Disable
[S] Save Settings
[D] Download Image Now
[L] Launch Existing Flash Resident Image Now
[E] Select Ether Device : FEC
[M] MMC and SD Utilities : ESDHC[1] is activated

Selection: d
+InitSpecifiedEthDevice
FECInit MAC ADDR 0:4:9f:1:1b:88
FEC is linked, Speed 100Mbps , Full Duplex
INFO: Fast Ethernet controller initialized.
INFO: MAC address: 0-4-9f-1-1b-88
-BLMenu .
INFO: Using device name: 'MX517048'
+EbootSendBootmeAndWaitForTftp
Sent BOOTME to 255.255.255.255
Sent BOOTME to 255.255.255.255
Sent BOOTME to 255.255.255.255
Sent BOOTME to 255.255.255.255
Sent BOOTME to 255.255.255.255
Sent BOOTME to 255.255.255.255
Sent BOOTME to 255.255.255.255
Sent BOOTME to 255.255.255.255
Sent BOOTME to 255.255.255.255
Sent BOOTME to 255.255.255.255
Packet has the following data:
boot.bin[NULL]octet[NULL]blksize[NULL]1024[NULL]
TFTP packet could have 2 name/value pairs
Locked Down Link 1
Src IP 192.168.5.45 Port Dest IP 192.168.5.20 Port Default TFTP block size set to: 512 bytes
This TFTP packet contains 1 options.
We currently only look at the first and expect it to be BLKSIZE.
The packet's option name is blksize.
The option's value is 1024
with a value that is in range.
BLKSIZE will be adjusted to 1024.
EthDown::TFTPD_OPEN::boot.bin
An OACK packet is the proper acknowledgement
-EbootSendBootmeAndWaitForTftp

BL_IMAGE_TYPE_BIN

INFO: OEMMultiBINNotify (dwNumRegions = 1, dwRegionStart = 0x9faa0000).
INFO: OEMVerifyMemory (CA = 0x9faa0000, PA = 0x1ffa0000, length = 0x6284480)
ERROR: Invalid address range.
!OEMVERIFYMEMORY: Invalid image
INFO: OEMReportError Reason 0xfffffff7

Can u suggest me

1.If there is any way to load the NK.bin in debug mode?

2.Reason for hang issue during booting in release mode?

Regards,
Praveen

0 项奖励
回复