Why does the dynamic linker skip the video-codecs that are part of libfslcodec?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Why does the dynamic linker skip the video-codecs that are part of libfslcodec?

882 次查看
catwich
Contributor I

Hi everybody,

I am currently working on integrating the Freescale gstreamer-0.10 plugins with debian wheezy armhf. Packages for both the gstreamer plugins and libfslcodec are basically done. The problem I am now stuck with is getting it to actually work.

I tried the test binary "test_mp3_dec_arm11_elinux_fhw" that is part of libfslcodec on my system, and I end up with his error message:

./test_mp3_dec_arm11_elinux_fhw: error while loading shared libraries: lib_mp3_dec_arm11_elinux.so.2: cannot open shared object file: No such file or directory

I examined the linker cache with ldconfig -p, and found the library is known, and has the right name:

llib_mp3_dec_arm11_elinux.so.2 (libc6) => /usr/lib/lib_mp3_dec_arm11_elinux.so.2

Using LD_DEBUG=libs, I found that the linker looks at the library,

trying file=/usr/lib/lib_mp3_dec_arm11_elinux.so.2

only to then continue and state that the it could not be found. I suspect the linker skips the library on purpose. But how can I find out why?


In case you want to see for yourself, the packages are in this repo:

deb Index of /BSP:/Cubox-i/Debian_Wheezy ./

mind that libfslcodec installs to /usr/lib/imx-mm/*/; I was moving the libs to /usr/lib manually to ease testing.

标签 (3)
0 项奖励
回复
0 回复数