Why and where we need to use system MCU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Why and where we need to use system MCU

1,120 次查看
mohsengh
Contributor III

Hello Dears

As we can see in following two blocks, We can use system MCU in mid to high infotainment.

but in entry one it is removed.

Can every on tell me Where we need to use system MCU?

As there is a tight requirement of vehicle interface to have very low standby current (as low as 100's uAs), is the role of this MCU for Manage system power and communicate to the vehicle bus?

Can iMX6solox meet this requirement without system MCU?

mid.PNG

entry.PNG

best regards

标签 (1)
0 项奖励
回复
2 回复数

1,045 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Hello Mohsen,

Can every on tell me Where we need to use system MCU?

ANSWER.  It is not like you need to use the System MCU,  the idea it is that this device offloads the CAN traffic and only pay attention to those messages that need to be taken care from the main processor.  So I would said it is not needed, just to provide an idea of how you can came to a solution when the CAN messages or the amount of CAN ports are not enough in the main processor.

As there is a tight requirement of vehicle interface to have very low standby current (as low as 100's uAs), is the role of this MCU for Manage system power and communicate to the vehicle bus? ANSWER. Yes This can be another option to add the System MCU.

Can iMX6solox meet this requirement without system MCU? ANSWER. Yes

1,045 次查看
mohsengh
Contributor III

Dear james

Thank you for your valuable response.

0 项奖励
回复