Why all the i.mx6 UltraLite part numbers operate at 528MHz and nothing operates at 696MHz?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why all the i.mx6 UltraLite part numbers operate at 528MHz and nothing operates at 696MHz?

948 Views
mahmoud_tolba
Contributor I

According to the product page of i.MX 6UltraLite Processor it operates at 696MHz but when I checked the datasheets of both consumer products and industrial products I found that all the part numbers operate at 528MHz ONLY?! Although

it is mentioned in the Part Number Nomenclature that there are 696MHz products!

Maybe future products?!

pastedImage_3.png

Could you explain this, please?

Labels (1)
0 Kudos
Reply
1 Reply

885 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mahmoud

one can find them in Buy/Parameters tab (MCIMX6G1AVM07AB)

i.MX 6UltraLite Applications Processor | Single Arm® Cortex®-A7 @ 696 MHz |NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply