Where to find HAB4_API.pdf for HAB?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where to find HAB4_API.pdf for HAB?

3,403 Views
zhongjianliang
Contributor I

Can anyone share / send me the "HAB4_API.pdf" file?

I have read a lot of documents and posts, that mentioned this document, which is supposed to be in the CST, but  it is not there anymore in the cst-2.3.3 package.

Could anyone tell me where to find this document?

I need to interpret the hab_status output.

Thank you very much!

Labels (1)
Tags (3)
0 Kudos
Reply
2 Replies

3,035 Views
paulstoffregen
Contributor III

In case anyone finds this old question, CST 3.3.0 and 3.3.1 do have HAB4_API.pdf in the "docs" folder.

0 Kudos
Reply

3,164 Views
igorpadykov
NXP Employee
NXP Employee

Hi Zhongjian

please create service request.

https://community.nxp.com/docs/DOC-329745 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply