Where to find HAB4_API.pdf for HAB?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where to find HAB4_API.pdf for HAB?

3,394件の閲覧回数
zhongjianliang
Contributor I

Can anyone share / send me the "HAB4_API.pdf" file?

I have read a lot of documents and posts, that mentioned this document, which is supposed to be in the CST, but  it is not there anymore in the cst-2.3.3 package.

Could anyone tell me where to find this document?

I need to interpret the hab_status output.

Thank you very much!

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

3,026件の閲覧回数
paulstoffregen
Contributor III

In case anyone finds this old question, CST 3.3.0 and 3.3.1 do have HAB4_API.pdf in the "docs" folder.

0 件の賞賛
返信

3,155件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Zhongjian

please create service request.

https://community.nxp.com/docs/DOC-329745 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信