Where is android 4.4.3 patch code for i.MX6.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is android 4.4.3 patch code for i.MX6.

ソリューションへジャンプ
4,626件の閲覧回数
satoshiazami
Contributor II

Hello All,

I want to build a Android 4.4.3 (or 4.4.2 ) for i.mx6.

I am reading a Android_User's_guide.pdf of android_kk4.4.3_2.0.0_ga_doc.tar.gz.

in that documents, "Patch code for i.MX" of Section 3.2.

in that sections,That document mentioned below.

 >1. Assume you have unzipped the i.MX Android release package to /opt/android_KK4.4.3_2.0.0-ga_source.

But I am not able to find out android_KK4.4.3_2.0.0-ga_source.xxx .

How can I take that file or package from there ?

Note:

 I could find another version of 6.0 and above. in NXP web site. it is below.

https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-soft...

Thank you for your time!

Please advise.

Best Regards,

Azami

ラベル(1)
0 件の賞賛
返信
1 解決策
4,388件の閲覧回数
satoshiazami
Contributor II

My inquiry is same as #343575.‌

I will access to local FAE.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,388件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   I've sent You link via e-mail


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,977件の閲覧回数
sfX
Contributor I

Hi I need KK4.4.3_2.0.1-ga_core_source.tar.gz as well pls

0 件の賞賛
返信
4,388件の閲覧回数
albert_zhang
Contributor II

Hi,

   Could you send the link to me? And should I do other works before you send? If i need, please tell me.

Thanks,

albert

0 件の賞賛
返信
4,388件の閲覧回数
satoshiazami
Contributor II

I'm sorry very late reply. I can use it !

Thank you !

So, Close this.

0 件の賞賛
返信
4,389件の閲覧回数
satoshiazami
Contributor II

My inquiry is same as #343575.‌

I will access to local FAE.

0 件の賞賛
返信