Where can I obtain the source code mxc_mcc_tty_test.c?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can I obtain the source code mxc_mcc_tty_test.c?

6,739件の閲覧回数
jingyangxie
Contributor V

Can anyone can send me source code(mxc_mcc_tty_test.c) of the demo mxc_mcc_tty_test.out ?

ラベル(2)
0 件の賞賛
返信
11 返答(返信)

6,285件の閲覧回数
qinghuazhu
Contributor III

you can get mxc_mcc_tty_test.c from

tmp/work/imx6ulevk-poky-linux-gnueabi/imx-test/1_5.4.1-r0/imx-test-5.4.1/test/mxc_mcc_tty_test

bitbake imx-test

6,285件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi jingyang,

mcc tty driver on latest kernel location :

     => drivers/char/imx_amp/imx_mcc_tty.c

Regards,

Aravinth

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

6,285件の閲覧回数
jingyangxie
Contributor V

Hi,aravinthkumar

   what's the version of the lastest kernel location you said ? in the BSP 4.1.15,I can't find the imx_mcc_tty.c in the directory drivers/char/imx_amp

0 件の賞賛
返信

6,285件の閲覧回数
jingyangxie
Contributor V

Hi,aravinthkumar

   in BSP 4.1.15, the file is list as follow:

pastedImage_0.png

Can you tell me which version you use ?

0 件の賞賛
返信

6,285件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi jingyang,

kernel version : 3.14.28

Regards,

Aravinth

0 件の賞賛
返信

6,283件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi,

Attached files are there in new kernel.

Regards,

Aravinth

0 件の賞賛
返信

6,278件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jingyang

please look at sect.53.3 Source Codes attached Linux Manual

imx6sx mcc tty driver : drivers/char/imx_mcc/imx_mcc_tty.c

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

6,278件の閲覧回数
jingyangxie
Contributor V

Hi,igorpadykov

    what does 53.3 mean? The BSP I use is 4.1.15,and I can't find the file imx_mcc_tty.c in the directory drivers/char/imx_mcc

0 件の賞賛
返信

6,278件の閲覧回数
jingyangxie
Contributor V

Hi,igorpadykov

    what's the linux manual you refered to above ,Please give more details,thanks!

0 件の賞賛
返信

6,278件の閲覧回数
jingyangxie
Contributor V

没有人做过imx6SX的多核通信吗?M4发给A9的数据,A9核的应用程序如何获取这些数据?

0 件の賞賛
返信

6,278件の閲覧回数
jingyangxie
Contributor V

MARK一下

0 件の賞賛
返信