Question, i.MX6SL PRESS_TIME configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX6SL PRESS_TIME configuration

2,145 Views
Aemj
Contributor IV

Dear team,

I would like to ask about PRESS_TIME bit field in SNVS_LPCR Register of i.MX6SL.

My customer is trying to change PRESS_TIME bit in SNVS_LPCR Register of i.MX6SL, but they cannot change it.

According to the following community thread, it seems to state that users cannot change PRESS_TIME.

Correct?

Configure SNVS Power Key

My customer wants to achieve the feature of power-down after 10 Sec power-switch-push as a feature of their product.

Please let me know if you have any ideas to achieve the feature.

Thanks,

Miyamoto

Labels (1)
0 Kudos
Reply
4 Replies

2,031 Views
Yuri
NXP Employee
NXP Employee

Hello,

  This is a documentation issue - correct bit fields description may be found in

Security Reference Manual for i.MX 6SoloLite. Bits 16:31 of  SNVS_LPCR are

reserved.
   External schematic is needed "to achieve the feature of power-down
after 10 Sec power-switch-push".

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,031 Views
Aemj
Contributor IV

Hi Yuri,

Do you mean that BTN_PRESS_TIME bit field does not exist?

Can you show me the example of the external schematic?

Thanks,

Miyamoto

0 Kudos
Reply

2,031 Views
Yuri
NXP Employee
NXP Employee

Yes, BTN_PRESS_TIME bit field does not exist.

Regards,

Yuri.

0 Kudos
Reply

2,031 Views
Aemj
Contributor IV

Hi Yuri,

If the button press time cannot be changed, is it possible to disable the long press feature?

The customer thinks that they can control it by their software?

Thanks,

Miyamoto

0 Kudos
Reply