Where can I find yocto BSP image and boot switch setting suitable for older IMX8M Mini EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I find yocto BSP image and boot switch setting suitable for older IMX8M Mini EVK

1,032 Views
leolarrel
Contributor I

Morning NXP world.

I need some help. I have one very old IMX8M Mini EVK board. board version is "SCH-31407 REV A" . PCB board color is black , not Green, and boot switch is 8 pin only , not 10 pin.

Where can I find yocto BSP image and boot switch setting suitable for this version of EVK ? I try to use yocto bsp version 'L4.14.98_2.0.0_ga_images_MX8MMEVK' and I can not boot on.

Thank you.

Leo

Labels (1)
0 Kudos
Reply
1 Reply

943 Views
shivanipatel
Senior Contributor II

Hi leolarrel@gmail.com‌,

You can find the boot mode settings on the board itself. They have given the boot mode settings table on the board.

For the images concern, all the supported Linux BSP for i.MX8M Mini EVK can be run on the board (black as well as green). You can find the Linux BSP and its documents from this link.

Hope this will help you.

If you still face any issue, please let us know.

Regards,

Shivani

0 Kudos
Reply