When u-boot jump to serial downloader mode in u-boot?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

When u-boot jump to serial downloader mode in u-boot?

跳至解决方案
2,249 次查看
kanoumamoru
Contributor III

Hello commuity,

 

I have one question concern with low level boot sequence.

 

Environment :

 - i.MX6DL @800MHz

 - DDR3 x 4pcs. (64bit bus)

 - SPI-NOR (u-boot and kernel)

 - eMMC (RootFS)

 

When SPI-NOR boot is selected:

  i.e. BOOT_MODE[1:0]=Internal Boot, BOOT_CFG1[7:4]=Serial ROM(SPI)

 

In this case, the system boot up sequence is as following :

  1. ROM code copy 4K byte data (include IVT and DCD table) from
      SPI-NOR to OCRAM.
  2. Init the DDR base on the DCD table settings.
  3. Copy and Load the u-boot form SPI-NOR to DDR.
  4. Jump to DDR to executes the u-boot.

 

A piece of DDR  was broken after ESD test, so DDR stress test became fail.

In other word, maybe above process 3, 4 (i.e.Copy and Load the u-boot / jump to DDR address) is not executed.

[Question]
In this case, the i.MX6 ROM BIOS will transition to the serial download mode?

 

Best Regards,

Kanou

标签 (3)
0 项奖励
回复
1 解答
1,970 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kanou

you are right: in this case i.MX6 ROM BIOS will transition to the serial download mode.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,970 次查看
kanoumamoru
Contributor III

Hi Igor,

Thank you for replying.

My customer say:

If possible, Would you tell me how serial download mode is determined by the BIOS.

What kind of logic does it change in a serial downloading mode in?

For example, jump to exception interrupt handler, DDR CRC check error, ....

Best Regards,

kanou

0 项奖励
回复
1,970 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kanou

yes ROM executes jump to exception interrupt handler.

Best regards
igor

0 项奖励
回复
1,971 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kanou

you are right: in this case i.MX6 ROM BIOS will transition to the serial download mode.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复