When the IMX6 decoding AVC format is very high probability will be stuck?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

When the IMX6 decoding AVC format is very high probability will be stuck?

1,963件の閲覧回数
fdact
Contributor I

Hi,

   The problem on imx6 sabresd_6dq  with android 4.2.2 and kernel 3.0.35.

   Log print out a lot of the follow contents:
   W/MediaPlayer( 3976): info/warning (3, 0)
   E/OMXCodec( 2254): [OMX.Freescale.std.video_decoder.avc.v3.hw-based] dequeueBuffer failed w/ error 0xfffffff0
   I/MediaPlayer( 3976): Info (3,0)

Thanks.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,749件の閲覧回数
art
NXP Employee
NXP Employee

Actually, this is the effect of some memory segmentation issue of the 3.0.35 kernel. Migrating to later BSP with later kernel revision should fix the issue.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,749件の閲覧回数
fdact
Contributor I

Can you kindly tell me which kernel version can be used on Android4.2.2? where to download? Can I only update kernel for my android system?

Thanks.

0 件の賞賛
返信

1,749件の閲覧回数
art
NXP Employee
NXP Employee

Q. Can I only update kernel for my android system?

A. No, it's not possible to only update the kernel. You have to completely migrate to later Android. Better to use the latest Marshmallow 6.0.1 BSP.

0 件の賞賛
返信