What value resistor should pull WDOG_B high?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What value resistor should pull WDOG_B high?

Jump to solution
2,630 Views
adevries
Contributor V

Hello,

In the i.MX 8M Mini hardware developer's guide, table 8, it suggest to pull GPIO1_IO02 (WDOG_B, ball AG13) high with a 100k ohm pull-up resistor. However, in section 5.5 of the same document, Note 2 says to pull the pin high with a 4.7k ohm resistor. Which value is actually recommended?

Thanks

Labels (1)
0 Kudos
Reply
1 Solution
2,491 Views
igorpadykov
NXP Employee
NXP Employee

Hi adevries 

100k ohm is sufficient, also one can use internal pull-up as described in

attached i.MX8M Mini EVK schematic p.12.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
2,492 Views
igorpadykov
NXP Employee
NXP Employee

Hi adevries 

100k ohm is sufficient, also one can use internal pull-up as described in

attached i.MX8M Mini EVK schematic p.12.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------