What value resistor should pull WDOG_B high?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What value resistor should pull WDOG_B high?

跳至解决方案
2,627 次查看
adevries
Contributor V

Hello,

In the i.MX 8M Mini hardware developer's guide, table 8, it suggest to pull GPIO1_IO02 (WDOG_B, ball AG13) high with a 100k ohm pull-up resistor. However, in section 5.5 of the same document, Note 2 says to pull the pin high with a 4.7k ohm resistor. Which value is actually recommended?

Thanks

标签 (1)
0 项奖励
回复
1 解答
2,488 次查看
igorpadykov
NXP Employee
NXP Employee

Hi adevries 

100k ohm is sufficient, also one can use internal pull-up as described in

attached i.MX8M Mini EVK schematic p.12.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
2,489 次查看
igorpadykov
NXP Employee
NXP Employee

Hi adevries 

100k ohm is sufficient, also one can use internal pull-up as described in

attached i.MX8M Mini EVK schematic p.12.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------