What the relation of sleep mode in hardware?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What the relation of sleep mode in hardware?

1,169 Views
wangvictor
Contributor III

Hi All,

I'm trying to using the sleep mode and wake it on the enternet(wol).

For sleep mode I'm using this commend : echo mem > /sys/power/state

For my hardware I have to understand how is sleep mode doing with the hardware.

To know that my hardware is support to this ability or not.

Anyone can give me the suggestion?

Or any document to let me read.

Thanks in Advanced!

0 Kudos
Reply
1 Reply

1,020 Views
b36401
NXP Employee
NXP Employee

In sleep mode PLLs and crystal oscillator are disabled.
As for Linux details you can refer to i.MX 6 Linux Reference Manual:
https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/i.mx-applicatio...

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply