IMX6ULL and DDR3L frequency related query?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6ULL and DDR3L frequency related query?

1,356件の閲覧回数
ramesh6663
Contributor III

In the EVK design have 1 DDR3 DRAM chip which is DDR3-1600. However, the datasheet of iMX6ULL says it only support DDR3-800, which means the bus frequency can only be 400Mhz. I am not sure how to use a higher speed memory with a lower speed CPU. When write data, that may be OK. But when read data, the data strobe is sent by DDR3-1600, which should be 800Mhz. How does it work with iMX6ULL 400Mhz bus frequency?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,074件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

for more detailed information about this, pls refer to the document as below:

https://community.nxp.com/docs/DOC-333791 

0 件の賞賛
返信