What the image processing capability of iMx8 processor?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What the image processing capability of iMx8 processor?

2,098 次查看
zcjiser_cn
Contributor I

Hi,
I'm assess the iMx8's specification for 4K@60 video processing. I have follow questions:

1. How to Scaling Video of 1080P@60 to 4K@60 on iMx8? is there any hardware module to use?
2. how many H.265/264 streams can be decoded at same time?

Is there any document describe the iMx8's Image processing capability?

0 项奖励
回复
3 回复数

2,079 次查看
zcjiser_cn
Contributor I

Thanks!

I read the sect.15.4 Imaging Subsystem.

I note that the ISI can only do down scailing.

If I want scaling up video(1080P@60 upscaling to 4K@60), should I can use the ISI to do it?

Best regards

zcjiser_cn

 

0 项奖励
回复

2,088 次查看
igorpadykov
NXP Employee
NXP Employee

Hi zcjiser_cn

 

general figures can be found in

i.MX 8QuadXPlus and 8DualXPlus Industrial Applications Processors - Data Sheet

sect.15.4 Imaging Subsystem  i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual

 

Best regards
igor

0 项奖励
回复

2,081 次查看
zcjiser_cn
Contributor I
 
0 项奖励
回复