Hi,
I am unable to build image for the default NXP release of 4.1.15.2.0.0 (Linux Kernel Version – Krogoth).
Build Steps:
The steps that were used for kicking off the build are the following.
repo init -u https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp.git -b imx-4.1-krogoth -m imx-4.1.15-2.1.1.xml
repo sync
DISTRO=fsl-imx-fb MACHINE=imx6ulevk source fsl-setup-release.sh -b build-4.1.15.2.0.0-imx6ulevk-dir
bitbake core-image-base
Build Errors:
ERROR: firmware-imx-1_5.4-r0 do_fetch: Fetcher failure: Unable to find revision 951c1363abe95dd75ab3e9447f640d7807240236 in branch master even from upstream
ERROR: firmware-imx-1_5.4-r0 do_fetch: Function failed: Fetcher failure for URL: 'git://github.com/NXP/imx-firmware.git;protocol=https;branch=master;destsuffix=imx-firmware;name=imx-firmware'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/jkareem/testing/ test-default-krogoth/build-4.1.15.2.0.0-imx6ulevk-dir/tmp/work/cortexa7hf-neon-mx6ul-poky-linux-gnueabi/firmware-imx/1_5.4-r0/temp/log.do_fetch.31430
ERROR: Task 1070 (/home/jkareem/testing/ test-default-krogoth/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/firmware-imx/firmware-imx_5.4.bb, do_fetch) failed with exit code '1'
Just wondering, whether, you have encountered this problem and have any solution for it?.
With Regards,
Jameel Basha