What the image processing capability of iMx8 processor?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What the image processing capability of iMx8 processor?

2,125件の閲覧回数
zcjiser_cn
Contributor I

Hi,
I'm assess the iMx8's specification for 4K@60 video processing. I have follow questions:

1. How to Scaling Video of 1080P@60 to 4K@60 on iMx8? is there any hardware module to use?
2. how many H.265/264 streams can be decoded at same time?

Is there any document describe the iMx8's Image processing capability?

0 件の賞賛
返信
3 返答(返信)

2,106件の閲覧回数
zcjiser_cn
Contributor I

Thanks!

I read the sect.15.4 Imaging Subsystem.

I note that the ISI can only do down scailing.

If I want scaling up video(1080P@60 upscaling to 4K@60), should I can use the ISI to do it?

Best regards

zcjiser_cn

 

0 件の賞賛
返信

2,115件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi zcjiser_cn

 

general figures can be found in

i.MX 8QuadXPlus and 8DualXPlus Industrial Applications Processors - Data Sheet

sect.15.4 Imaging Subsystem  i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual

 

Best regards
igor

0 件の賞賛
返信

2,108件の閲覧回数
zcjiser_cn
Contributor I
 
0 件の賞賛
返信