What the NOR flash supports imx6 processor for downloading U-boot?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What the NOR flash supports imx6 processor for downloading U-boot?

1,496 Views
rustemkhakimov
Contributor I

Hi,

What the NOR flash supports imx6 processor for downloading U-boot?

Labels (1)
Tags (3)
0 Kudos
Reply
2 Replies

1,205 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Gary has given the reply to you. Here you can refer to our i.mx6 reference board design in our community. You can refer to the board design in our website i.MX6Q|i.MX 6Quad Processors|Quad Core|NXP . There are 32M nor falsh and 4M nor flash in our reference design.

M29W256GL7AN6E

M25P32-VMW3TGB

Have a nice day

Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,205 Views
gary_bisson
Senior Contributor III

Hi,

You can have a look at the BD-SL-i.MX6 (SabreLite) schematics/documentation since it boots from NOR:

https://boundarydevices.com/product/sabre-lite-imx6-sbc/ 

The part used is the SST25VF016B.

Regards,

Gary