Error msg related to boot cmd in the saberlite imx6 board:

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error msg related to boot cmd in the saberlite imx6 board:

1,163件の閲覧回数
rajanikiranbr
Contributor I

In saberlite Imx6 board when i am running the boot cmd able to see the following error msg:

MMC Device 2 not found
no mmc device at slot 2

MMC read: dev # 0, block # 2048, count 8192 ... 8192 blocks read: OK
Wrong Image Format for bootm command
ERROR: can't get kernel image!

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,056件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Here you also need to check the boot up command lines setting in the u-boot.

Hope this can do help for you

Have a nice day

Dan

0 件の賞賛
返信

1,056件の閲覧回数
gary_bisson
Senior Contributor III

Hi,

Looks like what's on your SD card is corrupted. Please make sure to properly download and flash one of our images:

http://boundarydevices.com/imx6-builds/ 

Also, all our latest images require to upgrade to latest U-Boot, make sure you have the right version:

https://boundarydevices.com/u-boot-v2016-03/ 

Regards,

Gary

0 件の賞賛
返信