What´s needed for making Android Applications on i.MX53?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What´s needed for making Android Applications on i.MX53?

1,075 Views
RobertBagge
Contributor I

This is my first time developing applications for a quick start board and I am wondering what is different from "ordinary" applications development.

I have a i.MX53 board with a 5" touchscreen attached to it. The OS installed is Android.

Do you know if I can develop applications to the quick start board in the same way I do for Android Cellphones (Mac OS, Eclipse, debugging through device) or if I need some special software/drivers/OS on my development computer to make it happen?

Thanks for your help!

//Robert

0 Kudos
Reply
2 Replies

1,038 Views
RobertBagge
Contributor I

Okay, that´s great!

Thanks a lot for the quick reply.

0 Kudos
Reply

1,038 Views
daiane_angolini
NXP Employee
NXP Employee

if you want to create a "simple" application, like a to-do list manager, for example, you will need nothing special.

if you want to create some kind of GPS rellated app, you will need to control GPS driver/server

But, in fact, you will develop an android application for imx53qsb as any "ordinary" application for Android Cellphones.

0 Kudos
Reply