We develop one i.MX53 board which integrated OV3640 CMOS image sensor connected with CSI0 port. And get the driver from the L2.6.35_11.09.01_ER_source_bundle.tar.gz package. OV3640 works but the image is bad in color.
I inputed the gstreamer command line as followings:
gst-launch -v mfw_v4lsrc capture-width=640 capture-height=480 ! mfw_v4lsink
I recorded the video on the screen using my mobile phone and attached. The image's shape was clear but the color was bad. The colorful bar was flickering and shinning. Whether I have some mistake on the color format?
Can anybody help me for this problem? Thank you!
dmesg is normal. the ipu error is not a problem
I could not see your movie.
I think it´s a good idea take a scope and double check if your hardware is OK
and unfortunately, i have no idea how to use a scope and debug hardware =P
Dear Daiane,
Here is the movie I made.
I am wondering if there is some hardware problems in my board?
The dmesg log shows little information:
"
NV12
mxc_ipu mxc_ipu: IDMAC20's EBA0 is not 8-byte aligned
mxc_ipu mxc_ipu: IDMAC20's EBA1 is not 8-byte aligned
mxc_v4l_close: release resource
"
I don´t see anything on your log......
is LVDS´s pixclock right?
If you make a movie, can the movie be played on your PC?
Anything else from dmesg?
I believe it means the plugins feel difficult to scale the 640x480 images to the 1024x768 screen.
I changed the command line to be :
gst-launch -v --gst-debug=2 mfw_v4lsrc capture-width=640 capture-height=480 ! queue ! mfw_isink disp-width=640 disp-height=480
the warning disappeared. Please see the attached log.
what does it mean?
mfw_v4lsink mfw_gst_v4l.c:1357:mfw_gst_v4l2_display_init: Wrong display width information
Thank you!
Following is the gst-launch log:
root@freescale ~$ gst-launch -v --gst-debug=2 mfw_v4lsrc capture-width=640 ca>
MFW_GST_V4LSRC_PLUGIN 2.0.3 build on Mar 1 2012 13:44:16.
MFW_GST_V4LSINK_PLUGIN 2.0.3 build on Mar 1 2012 13:44:21.
Setting pipeline to PAUSED ...
/GstPipeline:pipeline0/MFWGstV4LSrc:mfwgstv4lsrc0.GstPad:src: caps = video/x-raw-yuv, format=(fourcc)NV12, width=(int)640, height=(int)480, framerate=(fraction)30/1, pixel-aspect-ratio=(fraction)1/1
Pipeline is live and does not need PREROLL ...
Setting pipeline to PLAYING ...
0:00:00.244215417 2192 0x16050 WARN bin gstbin.c:2312:gst_bin_do_latency_func:<pipeline0> failed to query latency
New clock: GstSystemClock
0:00:00.456938145 2192 0xe87b0 WARN mfw_v4lsink mfw_gst_v4lsink.c:1217:mfw_gst_v4lsink_set_format: set to nv12 mode
/GstPipeline:pipeline0/MFW_GST_V4LSINK_INFO_T:mfw_gst_v4lsink_info_t0.GstPad:sink: caps = video/x-raw-yuv, format=(fourcc)NV12, width=(int)640, height=(int)480, framerate=(fraction)30/1, pixel-aspect-ratio=(fraction)1/1
full screen size:1024x768
0:00:00.460228732 2192 0xe8ae0 WARN mfw_v4lsink mfw_gst_v4l.c:1357:mfw_gst_v4l2_display_init: Wrong display width information
0:00:00.460397355 2192 0xe8ae0 WARN mfw_v4lsink mfw_gst_v4l.c:1361:mfw_gst_v4l2_display_init: Wrong display height information
[V4L Update Display]: left=0, top=0, width=1024, height=768
0:00:00.460764975 2192 0xe87b0 WARN mfw_v4lsink mfw_gst_v4lsink.c:1217:mfw_gst_v4lsink_set_format: set to nv12 mode
>>V4L_SINK: Actually buffer status:
hardware buffer : 12
software buffer : 0
Ok
So you think the error is not caused by any mismatch of configuration, right?
Please, let me see your debug log
gst-launch -v --gst-debug=2 (...)
In fact, I´m not sure about sensor-width property. I don´t use it.
You can set capture-mode=0 to get 640x480 from your camera
But, have you tried only:
gst-launch mfw_v4lsrc ! mfw_v4lsink
????
Thank you!
Is the mode which listed in ov3640.c as following:
enum ov3640_mode {
ov3640_mode_MIN = 0,
ov3640_mode_VGA_640_480 = 0,
ov3640_mode_QVGA_320_240 = 1,
ov3640_mode_XGA_1024_768 = 2,
ov3640_mode_QXGA_2048_1536 = 3,
ov3640_mode_NTSC_720_480 = 4,
ov3640_mode_PAL_720_576 = 5,
ov3640_mode_MAX = 5
};
By the way, what is the difference between the property "sensor-width" and "capture-width" of the plugin mfw_v4lsrc? Should I set the property “sensor-width" and "sensor-height"? (When I tried, no apparently difference on the screen)
OK, I will start a new topic for the VPU problem. Yes, it is very complex. Thank you!
Please, open a new topic for the VPU stuff. Network streaming is a very complex topic. Take a look on others conversations and try as much as you can.
Let´s keep this one for camera.
In your first command line (gst-launch -v mfw_v4lsrc capture-width=640 capture-height=480 ! mfw_v4lsink) there is no VPU reference. It´s a lookback camera -> display
Take a look on camera´s driver (on kernel, it should be something like ov3640.c) you will find any "supported capture mode".
For example, if you configure the camera with capture mode = 1, you will configure camera for 360X480@25FPS. If you configure all other parameters on gstreamer command line another way, you will get a bad picture on screen.
So, take a look on the "real supported" parameters, and make sure your camera configuration and command like match.
Daiane,
Thank you!
gst-launch-0.10 -v udpsrc port=5002 ! queue ! capsfilter caps="application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, profile-level-id=(string)420014, payload=(int)96" ! rtph264depay ! mfw_vpudecoder codec-type=std_avc ! queue ! mfw_isink sync=false
Used following command line as video streaming transmitter:
Daiane Angolini said:
Do you know if your "standard" camera capture mode is for 640X480?
The clock on the camera is right?
Do you know if your "standard" camera capture mode is for 640X480?
The clock on the camera is right?