What's IP Bus Means

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
8,448件の閲覧回数
jerryzhai
Contributor II

Dear Specialist:

In im6dl platform datasheet (IMX6SDLRM.pdf), there is a bus called IP bus.

My question is :

1. what this IP means, in other word, if IP is a abbreviation, what is its original words.

2. The functions and features of this IP Bus.

Thanks

ラベル(1)
1 解決策
6,853件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jerry

general meaning IP: intellectual property (IP) bus interface,

that is bus for some module. It may be useful to look at

Chapter 13 AHB to IP Bridge (AIPSTZ) IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
6,854件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jerry

general meaning IP: intellectual property (IP) bus interface,

that is bus for some module. It may be useful to look at

Chapter 13 AHB to IP Bridge (AIPSTZ) IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信