What's IP Bus Means

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What's IP Bus Means

跳至解决方案
8,391 次查看
jerryzhai
Contributor II

Dear Specialist:

In im6dl platform datasheet (IMX6SDLRM.pdf), there is a bus called IP bus.

My question is :

1. what this IP means, in other word, if IP is a abbreviation, what is its original words.

2. The functions and features of this IP Bus.

Thanks

标签 (1)
1 解答
6,796 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jerry

general meaning IP: intellectual property (IP) bus interface,

that is bus for some module. It may be useful to look at

Chapter 13 AHB to IP Bridge (AIPSTZ) IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
6,797 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jerry

general meaning IP: intellectual property (IP) bus interface,

that is bus for some module. It may be useful to look at

Chapter 13 AHB to IP Bridge (AIPSTZ) IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复