What's IP Bus Means

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What's IP Bus Means

Jump to solution
8,455 Views
jerryzhai
Contributor II

Dear Specialist:

In im6dl platform datasheet (IMX6SDLRM.pdf), there is a bus called IP bus.

My question is :

1. what this IP means, in other word, if IP is a abbreviation, what is its original words.

2. The functions and features of this IP Bus.

Thanks

Labels (1)
1 Solution
6,860 Views
igorpadykov
NXP Employee
NXP Employee

Hi jerry

general meaning IP: intellectual property (IP) bus interface,

that is bus for some module. It may be useful to look at

Chapter 13 AHB to IP Bridge (AIPSTZ) IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
6,861 Views
igorpadykov
NXP Employee
NXP Employee

Hi jerry

general meaning IP: intellectual property (IP) bus interface,

that is bus for some module. It may be useful to look at

Chapter 13 AHB to IP Bridge (AIPSTZ) IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply