What is the recommendation when using JTAG boundary scan but not using PCIe on iMX7 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the recommendation when using JTAG boundary scan but not using PCIe on iMX7 ?

2,092件の閲覧回数
wad1
Contributor III

We are using an iMX7 Dual SoC, and while we appreciate the inclusion of a PCIe interface we currently have no use for it in our design.  In Section 3.2 of the datasheet (iMX7Dual Family of Applications Processors Datasheet, Rev. 2, 06/2016), Table 5 recommends that if not using PCIe to leave a number of signals floating, and to tie PCIE_VP, PCIE_VP_RX, PCIE_VP_TX, PCIE_VPH, PCIE_VPH_RX, PCIE_VPH_TX, and PCIE_REXT to ground.

In Table 8 of the hardware development guide (Hardware Development Guide for i.MX7Dual and 7Solo Applications Processors, Rev. 0, 07/2016), note 5 says that if JTAG boundary scan is to be supported, the following supplies must be powered: PCIE_VP, PCIE_VPH, PCIE_VP_TX (the doc has a typo on that last signal name).

The question is, in the case of not using PCIe, but desiring to support boundary scan, exactly what should all the other pins be connected to ?

The literal interpretation of the documentation results in:

PCIE_VP  powered by LDO_1P0D

PCIE_VP_RX tied to ground

PCIE_VP_TX powered by LDO_1P0D

PCIE_VPH powered by VDDA_PHY_1P8

PCIE_VPH_RX tied to ground

PCIE_VPH_TX tied to ground

PCIE_REXT tied to ground

Is this correct ?

I'm assuming that since PCIE_VP, PCIE_VPH, and PCI_VP_TX are only used for infrequent JTAG, it is OK to only provide the internal LDO_1P0D regulator with minimal bypassing (0.22uF), and supply the PCIE_VPH supply from the +1.8V switch (VDDA_PHY_1P8) without bypassing.   MIDI is also powered down via the instructions in Table 5 of the datasheet.  Comments ?

ラベル(2)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

1,873件の閲覧回数
art
NXP Employee
NXP Employee

Actually, for reliable boundary scan operation, all of the PCIe PHY power rails should be supplied with their respective voltages: 1.0V for PCIE_VP, PCIE_VP_TX, PCIE_VP_RX, can be supplied from the LDO_1P0D, 1.8V for PCIE_VPH, PCIE_VPH_TX, PCIE_VPH_RX, can be supplied from VDDA_PHY_1P8. All other PCIe PHY signals should be left floating.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,873件の閲覧回数
cyuk
Contributor I

Hi (Artur),

How is the PCIE related to the JTAG in the SOLO version without PCIE? Should the power pins be floating?

0 件の賞賛
返信

1,873件の閲覧回数
wad1
Contributor III

Thanks for the prompt answer.  What about PCIE_REXT ?  Tie to ground or tie to ground through a resistor ?

0 件の賞賛
返信

1,873件の閲覧回数
art
NXP Employee
NXP Employee

Can be either grounded through a resistor or left floating. No direct connection to GND is allowed when the supply voltages are applied.

0 件の賞賛
返信