What is the real memory address with DDR contorller map

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the real memory address with DDR contorller map

1,436 Views
shangregister
Contributor II

HI all

I using imx8mq EVK and find the DDR memory A53 Address from 0x4000_0000 to FFFF_FFFF (3GB)

but what is the real address represent (like Row/Col/Bank/CS)??

Can i find it in the Applications Processors Reference Manual?

Hanson

Labels (1)
0 Kudos
Reply
2 Replies

1,254 Views
shangregister
Contributor II

Any body can help??

0 Kudos
Reply

1,254 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hanson

there are Address Map Registers  (ADDRMAP) described in sect

9.3.3.1.62 i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual

For selection row/columns one can use xls RPA tools described on

https://community.nxp.com/docs/DOC-340179 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply