What is the pin name of i.MX8M Mini SD3_RESET_B when boot from SDHC3?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What is the pin name of i.MX8M Mini SD3_RESET_B when boot from SDHC3?

跳至解决方案
1,123 次查看
m_c
Senior Contributor I

What is the pin name of i.MX8M Mini SD3_RESET_B when boot from SDHC3?

pastedImage_3.png

pastedImage_4.png

标签 (1)
0 项奖励
回复
1 解答
1,057 次查看
Yuri
NXP Employee
NXP Employee

 Hello,

 

  NAND_READY_B is used as SD3_RESET for SD3 boot.

Use "Boot device interface allocation" section in i.MX 8Mm Datasheet(s).

Also, i.MX Pins tool helps here.

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,058 次查看
Yuri
NXP Employee
NXP Employee

 Hello,

 

  NAND_READY_B is used as SD3_RESET for SD3 boot.

Use "Boot device interface allocation" section in i.MX 8Mm Datasheet(s).

Also, i.MX Pins tool helps here.

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 项奖励
回复