What is the pin name of i.MX8M Mini SD3_RESET_B when boot from SDHC3?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the pin name of i.MX8M Mini SD3_RESET_B when boot from SDHC3?

ソリューションへジャンプ
1,210件の閲覧回数
m_c
Senior Contributor I

What is the pin name of i.MX8M Mini SD3_RESET_B when boot from SDHC3?

pastedImage_3.png

pastedImage_4.png

ラベル(1)
0 件の賞賛
返信
1 解決策
1,144件の閲覧回数
Yuri
NXP Employee
NXP Employee

 Hello,

 

  NAND_READY_B is used as SD3_RESET for SD3 boot.

Use "Boot device interface allocation" section in i.MX 8Mm Datasheet(s).

Also, i.MX Pins tool helps here.

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,145件の閲覧回数
Yuri
NXP Employee
NXP Employee

 Hello,

 

  NAND_READY_B is used as SD3_RESET for SD3 boot.

Use "Boot device interface allocation" section in i.MX 8Mm Datasheet(s).

Also, i.MX Pins tool helps here.

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 件の賞賛
返信