What is the difference between the security zone on the i.MX8 vs the SEC module on the LS1046A?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the difference between the security zone on the i.MX8 vs the SEC module on the LS1046A?

1,144 Views
apache8080
Contributor I

I am comparing the i.MX 8 M Plus to the LS1046A and specifically wanted to know the difference between the two different security modules. I know both seem to have crypto accelerators and HW RNG's. Both also seem to allow secure boot but is there something that one has over the other.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,128 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

They are products focused to different segments for which it would be helpful to check your target application + the security features of your interest. For the security features, you may refer to the following documentation.

For LS1046A, please refer to the security reference manual, chapter 3.2 (Cryptographic engines implemented in SEC): https://www.nxp.com/docs/en/reference-manual/LS1046ASECRM.pdf

i.MX8M Plus, the security features are described in table 1 -> Security (Subsystem field): https://www.nxp.com/docs/en/data-sheet/IMX8MPIEC.pdf

 

Hope it helps!

 

BR,

Ivan.

 

 

 

0 Kudos
Reply