What is the difference between the security zone on the i.MX8 vs the SEC module on the LS1046A?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the difference between the security zone on the i.MX8 vs the SEC module on the LS1046A?

916件の閲覧回数
apache8080
Contributor I

I am comparing the i.MX 8 M Plus to the LS1046A and specifically wanted to know the difference between the two different security modules. I know both seem to have crypto accelerators and HW RNG's. Both also seem to allow secure boot but is there something that one has over the other.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

900件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

They are products focused to different segments for which it would be helpful to check your target application + the security features of your interest. For the security features, you may refer to the following documentation.

For LS1046A, please refer to the security reference manual, chapter 3.2 (Cryptographic engines implemented in SEC): https://www.nxp.com/docs/en/reference-manual/LS1046ASECRM.pdf

i.MX8M Plus, the security features are described in table 1 -> Security (Subsystem field): https://www.nxp.com/docs/en/data-sheet/IMX8MPIEC.pdf

 

Hope it helps!

 

BR,

Ivan.

 

 

 

0 件の賞賛
返信