What is processor System frequency and processor ARM frequency of iMX6?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is processor System frequency and processor ARM frequency of iMX6?

ソリューションへジャンプ
3,637件の閲覧回数
mohammedazlum
Contributor IV

Hello,

Please let me know that, What is processor System frequency and processor ARM frequency of iMX6?

I'm using iMX6 dual lite 800Mhz processor. Here what is System frequency and ARM frequency of iMX6 ?

Regards,

Azlum

ラベル(1)
1 解決策
3,463件の閲覧回数
Yuri
NXP Employee
NXP Employee

Yes, 528 MHz. Also, please refer to Chapter 18 (Clock Controller Module (CCM)) of the Reference
Manual.

~Yuri.

元の投稿で解決策を見る

5 返答(返信)
3,463件の閲覧回数
mohammedazlum
Contributor IV

Hello,

ARM frequency  is 800Mhz. But what is System Frequency ? And what is the difference between System frequency and ARM frequency of iMX6DL ?


Regards,

Azlum

0 件の賞賛
返信
3,463件の閲覧回数
Yuri
NXP Employee
NXP Employee

  System frequency - usually it is system bus frequency, which is equal DRAM frequency.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,463件の閲覧回数
mohammedazlum
Contributor IV

Dear Yuri,

Is this 528Mhz ? If yes, from where we are deriving 528Mhz ?

Regards,

Azlum

528Mhz.png

0 件の賞賛
返信
3,464件の閲覧回数
Yuri
NXP Employee
NXP Employee

Yes, 528 MHz. Also, please refer to Chapter 18 (Clock Controller Module (CCM)) of the Reference
Manual.

~Yuri.

3,463件の閲覧回数
mohammedazlum
Contributor IV

Thank you Yuri :smileyhappy:

0 件の賞賛
返信