i.MX6 for telephony application.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 for telephony application.

1,530件の閲覧回数
sumit8915
Contributor III

Hi,

  Have anybody used i.MX6 for telephony application.

  Is there any reference design which freescale has developed?

0 件の賞賛
返信
3 返答(返信)

1,327件の閲覧回数
art
NXP Employee
NXP Employee

There is the i.MX6 SABRE SDP reference design by Freescale. It allows a 3G module connection. It can run Android that supports the telephony features. I think, all this together can be considered as the telephony application reference. For more information, please refer to the i.MX6 SABRE SDP web page:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,327件の閲覧回数
sumit8915
Contributor III

Hi Artur,

 

    We don't want to include this feature via 3G module.

    Our design requirement is kind of Analog Telephone Adapter(ATA) which will incorporate the feature of connecting the Analog telephone to it and make the calls thorough VoIP.

    

0 件の賞賛
返信

1,327件の閲覧回数
sumit8915
Contributor III

Hi,

  Please Reply on this if anybody worked upon this or have any understanding.

0 件の賞賛
返信