What is processor System frequency and processor ARM frequency of iMX6?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is processor System frequency and processor ARM frequency of iMX6?

Jump to solution
3,574 Views
mohammedazlum
Contributor IV

Hello,

Please let me know that, What is processor System frequency and processor ARM frequency of iMX6?

I'm using iMX6 dual lite 800Mhz processor. Here what is System frequency and ARM frequency of iMX6 ?

Regards,

Azlum

Labels (1)
1 Solution
3,400 Views
Yuri
NXP Employee
NXP Employee

Yes, 528 MHz. Also, please refer to Chapter 18 (Clock Controller Module (CCM)) of the Reference
Manual.

~Yuri.

View solution in original post

5 Replies
3,400 Views
mohammedazlum
Contributor IV

Hello,

ARM frequency  is 800Mhz. But what is System Frequency ? And what is the difference between System frequency and ARM frequency of iMX6DL ?


Regards,

Azlum

0 Kudos
Reply
3,400 Views
Yuri
NXP Employee
NXP Employee

  System frequency - usually it is system bus frequency, which is equal DRAM frequency.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,400 Views
mohammedazlum
Contributor IV

Dear Yuri,

Is this 528Mhz ? If yes, from where we are deriving 528Mhz ?

Regards,

Azlum

528Mhz.png

0 Kudos
Reply
3,401 Views
Yuri
NXP Employee
NXP Employee

Yes, 528 MHz. Also, please refer to Chapter 18 (Clock Controller Module (CCM)) of the Reference
Manual.

~Yuri.

3,400 Views
mohammedazlum
Contributor IV

Thank you Yuri :smileyhappy:

0 Kudos
Reply