What is maximun resolution that i.MX6 Dual can manage with MiPi DSI?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is maximun resolution that i.MX6 Dual can manage with MiPi DSI?

Jump to solution
1,492 Views
jdepedro
Contributor IV

 Looking at the NXP documentation there is a mismatching or a typo, looking at the manuals:

"Programmable display resolutions, from 160x120(QQVGA) to 1280x720(XVGA)."

"Programmable display resolutions, from 160x120(QQVGA) to 1024x768(XVGA)"

Also seems like XVGA is not an standard format: wikipedia

Could you confirm what is the correct information? Thanks

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,217 Views
Yuri
NXP Employee
NXP Employee

Hello,

  "The maximum possible display resolution on the MIPI DSI interface of the i.MX6 [...] is 1280x720 pixels,

as specified in the Reference Manual document.

MIPI DSI max display resolution 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,218 Views
Yuri
NXP Employee
NXP Employee

Hello,

  "The maximum possible display resolution on the MIPI DSI interface of the i.MX6 [...] is 1280x720 pixels,

as specified in the Reference Manual document.

MIPI DSI max display resolution 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply