What is SE BLANK RITA decive?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is SE BLANK RITA decive?

ソリューションへジャンプ
10,335件の閲覧回数
YanjunLuo
Contributor IV

My new MX535 board is based on Quick Start RevB and use a new PMIC MC34709. I checked all voltages are ok, the 24MHz works too, but I set the boot mode to serial download, my PC always get the unknow device. I found when I send a reset a this time, the unknow USB device changes to "SE BLANK RITA" device, and no driver. Does anybody know what's wrong with it? What is SE BLANK RITA device? It looks like the MX535 works a little, but the USB device should be "Bulk IO Device".

Regards,

Yanjun Luo.

ラベル(1)
0 件の賞賛
返信
1 解決策
6,139件の閲覧回数
YanjunLuo
Contributor IV

I got answer from FAE today, RITA means i.MX53, it works, but need a driver. After install the right driver, the "Freescale i.MX53 USB BulkIO Device" is ready, and I can download software.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
6,140件の閲覧回数
YanjunLuo
Contributor IV

I got answer from FAE today, RITA means i.MX53, it works, but need a driver. After install the right driver, the "Freescale i.MX53 USB BulkIO Device" is ready, and I can download software.

0 件の賞賛
返信
6,139件の閲覧回数
Salma
Contributor I

If possible can you please share "SE BLANK RITA" device driver.

Regards,

Salma

0 件の賞賛
返信
6,139件の閲覧回数
YanjunLuo
Contributor IV

You just need install the Mfgtools driver. My problem is when I install the driver, I choosed a wrong folder.

Regards,

Yanjun Luo.

0 件の賞賛
返信