What is SE BLANK RITA decive?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is SE BLANK RITA decive?

Jump to solution
10,532 Views
YanjunLuo
Contributor IV

My new MX535 board is based on Quick Start RevB and use a new PMIC MC34709. I checked all voltages are ok, the 24MHz works too, but I set the boot mode to serial download, my PC always get the unknow device. I found when I send a reset a this time, the unknow USB device changes to "SE BLANK RITA" device, and no driver. Does anybody know what's wrong with it? What is SE BLANK RITA device? It looks like the MX535 works a little, but the USB device should be "Bulk IO Device".

Regards,

Yanjun Luo.

Labels (1)
0 Kudos
Reply
1 Solution
6,336 Views
YanjunLuo
Contributor IV

I got answer from FAE today, RITA means i.MX53, it works, but need a driver. After install the right driver, the "Freescale i.MX53 USB BulkIO Device" is ready, and I can download software.

View solution in original post

0 Kudos
Reply
3 Replies
6,337 Views
YanjunLuo
Contributor IV

I got answer from FAE today, RITA means i.MX53, it works, but need a driver. After install the right driver, the "Freescale i.MX53 USB BulkIO Device" is ready, and I can download software.

0 Kudos
Reply
6,336 Views
Salma
Contributor I

If possible can you please share "SE BLANK RITA" device driver.

Regards,

Salma

0 Kudos
Reply
6,336 Views
YanjunLuo
Contributor IV

You just need install the Mfgtools driver. My problem is when I install the driver, I choosed a wrong folder.

Regards,

Yanjun Luo.

0 Kudos
Reply