What if USB interface is not populated over Target board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What if USB interface is not populated over Target board

950 次查看
adityanagal
Contributor III

Hi ,

What I understood from the IMX6 reference manuals , In the bootstrap mode host and ROM communicates over serial download protocol over USB interface for flashing Uboot , kernel etc on boot device . What if the USB interface is not

populated over the target board. Then is there any way to flash the uboot , kerenel etc on boot device.

Please suggest.

0 项奖励
回复
2 回复数

876 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Hello Aditya,

if you are not using the USB then you can use the UART to download the code, but it is extremely slow a comparison with the USB port.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

876 次查看
adityanagal
Contributor III

Hi ,

How to use the UART instead of USB in Serial Download booting mode for firmware flashing . Is it possible to use UART in Serial download mode for firmware flashing ?

Regards,

Aditya Nagal

0 项奖励
回复